Other Parts Discussed in Thread: USB2ANY, DAC81416
Hello,
I'm evaluating the DAC81416EVM board. So far interfacing the DAC with an external microcontroller works fine. I manage to W/R register and output voltages on different channels. I compared performances by using the USB2ANY TI interface. I realise that the SPI clock provided by this interfaced is by default set to 45kHz while the speed of ths SPI clocl of my board is around 322kHz.
My question here is how to mange to reduce interferences induced by the SPI lines on the outputs when operating abovee 100kKz. I have a strong interest to use this DAC with a SPI clock of 20MHz.
Do you have any recommendation of length of cable that should be used in this condition?. Is there any termination network that you recommend that help to reduce the spike produced by the clock pluses when running at high speed?
best regards,
Fausto