Hi expert,
I am using ADS1216 and my test circuit is to sample a constant 0.147V DC voltage, but I get wrong digital code when I change the data rate of ADS1216 from 10SPS to 300SPS. Can you give me some suggestions on the possible reason cause this issue?
Below is my configuration.
- Input:0.147V dc
- REF: external 2.5V.
- Digital code output:
-
- about 500000 at 10SPS(this is correct based on 0.0147V dc input),
- about 300000 at 300SPS(this is wrong)
-
- Software register config are as below picture.
Thanks and best regards
Rachel