This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
also please refer to the following app note:
we have app note .
Dear Chen,
Thank you very much for your response. My concern is that it looks as though it doesn't do very well with frequencies below 100 kHz. The plot in Fig 5.4 concerns me - even for the "red" curve for low frequency settings. ALSO, I want raw data, not beam formed data.
Does TI offer some sort of truly sonar - or audio - data converter that simply amplifies and sends directly to A/D?
Thank you for your information,
Sarah Patch
Hi,
For your concern using AFE5809, on the Figure 19 section 5.4,
it does not cover very detail information,
for more detailed description as follows:
with INM capacitor (Cbypass) = 15nF, the LNA cutoff freq=100kHz
with INM capacitor (Cbypass) = 22nF, the LNA cutoff freq=70kHz
with INM capacitor (Cbypass) = 47nF, the LNA cutoff freq=33kHz
with INM capacitor (Cbypass) = 1uF, the LNA cutoff freq=2kHz
Notice: PGA_HPF_Disable='1', HPF_LNA="01"
Thank you!