Hi there,
got some trouble where I got sometimes an alarmout caused by AVss alarm. I want to understand it a bit more what perhaps helps so solve our problems.
- Threshold is -3.8V to -4.4V. What does it exactly mean in terms of time durations? How long needs my AVss (my setup uses -5V) over that threshold of -4.4V...-3.8V to be? nano, mikro, milli...seconds?
- So it could be that the AVss itself is over that threshold or its reference right?
- The reference is what exactly? AGNDx?
- Shouldnt I see something with the oscilloscope between AVss and GND (AGND and DGND connected together in my design) when the AMC is claming about AVss alarm?
I cannot measure something bad on the AVss pin but perhaps I`m searching in the wrong time scale. Would be interesting if also a short event like a Nanosecond would be enough to trigger the AVss alarm.
Thanks and cheers,
Markus