Other Parts Discussed in Thread: ADS1256, ADCPRO
Hello TI,
I am looking for the C code (or any programming language) running on the C55x DSP on the MMB0 board. I am familiar with the C55x DSP and CCS. I just need the source code and the project that contains the code that initialize the ADC.
I plan to use the ADS1256EVM board in a tester. I have implementing SPI code interface to the ADS1256 via the EVM board J2 connector. Enclosed is the wave form as I issue to reset the device. top 5 signals in white are digital waveform captured. Bottom 5 signals in blue are the same waveform in analog capture.
and below is the reset command done by the C55x on the MMB0 board
I don't know why after I issue the reset command, the DRDY (channel 7) continues to toggle. Also as I follow the same command sequence (captured on the logic analyzer) as the DSP initializes the ADC, I did not get back the same response. I am using SPI mode 1 (CPOL=0, CPHA=1) as implies in the ADS1256 datasheet page 6, figure 1. I tried SPI mode 0 also but I am not able to setup the ADC. I hope that the source code will shed some light on this.
I also looked for the ADS1256 programming guide of application notes (from a processor's perspective) and I could not find any. Please point me to the URL if these technical artifacts exist.
Thank you,
Sy