Hi Sir,
Would you pls help for below questions? Thanks.
1. The schematic as below is fine?
2. How to calculate I3? or it can ignore?
Thanks, Ian.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sir,
Would you pls help for below questions? Thanks.
1. The schematic as below is fine?
2. How to calculate I3? or it can ignore?
Thanks, Ian.
Hello,
1. I would suggest following the image below for connecting your device.
There is also a tech note on using the ADS7142 with a NTC that would be helpful here as well.
Some notes: the AINM pin needs to be grounded, it cannot be left floating, decoupling caps missing on power supply lines. SCL and SCA lines should be connected to the host. Also suggest to monitor BUSY pin.
2. the current to the input pin of the device is dynamic, it will change as the device samples and holds. you would need to take an average measurement of this current. Depending on why you want to measure this current, you could not worry about it
Regards
Cynthia