• TI Thinks Resolved

ADC08100EVM: Clock Out and Pin Diagram

Prodigy 50 points

Replies: 9

Views: 68

Part Number: ADC08100EVM

Hello,

I am having trouble finding information on the ADC08100EVM. I have the User's Guide, but this is missing some details. 

First, it mentions the clock output (J2) but never specifies what this signal will look like. Will it be identical to the clock input with a delay? 

Second, I would like to see a labelled schematic for the board. Specifically, I would like to see a table labeling each of the CMOS pins (J1). I do not have the TSW1400EVM and have no means of measuring the ADC output at this point. A similar question was raised here https://e2e.ti.com/support/data-converters/f/73/p/928986/3432060#3432060?jktype=e2e. The answer to that question attaches a link, but I am having trouble finding any such diagram there. 

If you could point me in the right direction to get things started, I would really appreciate it! Thank you!