Part Number: ADS1118
Hi Team
My customer is using ADS1118 and he wants to know the value of conversion error parameter for specific condition since the value in datasheet is measured by
different condition.
Is it possible to get the data for gain error, offset error and INL? for example, by simulation. Thanks.
Gain error
Offset error
INL
Condition
・Ambient temp:25℃
・power voltage:5.25V
・input signal:DC signal from OP amp
・Input serial resistor:3600Ω
・FSR:6.144V
・DR:250SPS
・input mode:single-end
Besides, the customer also wants to know if we have data showing relationship between input serial resistor and AD conversion error.
And if there is no data for parameter that the customer is asking above, could you tell me if we can get it by calculation.
Please let me know if you need more information.
Thanks.