Other Parts Discussed in Thread: LMK04828
Hello team,
Is there description for status LED mounted on DAC38RF80EVM?
Best regards,
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello team,
Is there description for status LED mounted on DAC38RF80EVM?
Best regards,
Taketo,
The only LED's that are truly assigned a task are D5, D4 and D3. D5 is USB power present, D4 reports if the PLL2 is locked inside the LMK04828 and D3 reports if PLL1 is locked inside the LMK04828. The other LED's are controlled by the FMC and the FPGA from the interface board used that is driving them. I think most of the current firmware is just turning these three on once the firmware is load. No status other than that.
Regards,
Jim