Other Parts Discussed in Thread: LMH5401, DAC38J84
Hi,
Our design use DAC37J82 with Rload=50ohm on each IOUTAP/N analog output.
Data input code is two complement (range: (-32k) to 32k)
IOUTP/N output current is 20mA (coarse_dac[3:0] =0xA, RBIAS = 1920ohm, VEXTIO=0.9V)
Measuring IOUTP/N on scope (1Mohm input resistance) shows that
Vdiff = 1V (as expected), however, both signals have min DCoffset of 130mV :
IOUTP/N signals voltages are oscillating between 0.13V-1.13V.
DCoffset is higher if coarse_dac[3:0] is higher then 0xA.
We tried to "play" with DC offset with config80[15], config8[12:0] registers....DC offset change was not enogh to make IOUTP/N signals voltages to be between 0V-1V.
Pls advise.
Thanks