Other Parts Discussed in Thread: ADS8688
Hi,
what's the difference between ADS8688 and ADS8688A? which part is recommended for new project?
Best Regards
Sean Zhang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Sean,
The ADS8688A is same as ADS8688 except the additional features:
1. More input ranges per channel:
ADS8688: ±10.24 V, ±5.12 V, ±2.56 V, 10.24 V, 5.12 V
ADS8688A: ±10.24 V, ±5.12 V, ±2.56 V, ±1.28 V, ±0.64 V, 10.24 V, 5.12 V, 2.56 V, 1.28 V
2. Alarm feature for input monitoring:
The ALARM allows the user to program individual high and low thresholds for each input channel and the ADC outputs a flag if the input exceeds the threshold set by the user in any direction.
Regards,
Dale