Hi TI,
I am working with the ADS1298 eight channel ECG IC. I am currently struggling with getting the DC lead off detection to work.
The configuration is measuring LeadI with the RA, LA and RL electrodes.
Below are examples of LeadI signal when one of the three electrodes are being removed: (Don't mind the poor quality of the signal view, as it is just to help with development). The signal is displayed in mV.
With no electrodes disconnected:
With the RA electrode disconnected:
With the LA electrode disconnected:
With the RL electrode disconnected:
// The behavior:
I was expecting the LeadI signal to be driven to one of the supply rails when either RA or LA was removed. Instead I am seeing some sort of oscillations..
Also when RL was removed I was expecting a lot of noise, but not a lot is picked up..
Can you tell me what behavior I should be seeing on LeadI when removing the electrodes?
The setup of all device registers is listed below.
// Setup of the IC:
The ADS1298 is set up to measure LeadI with the RA, LA electrodes which are attached to channel 8 at 250SPS.
It has RLD activated with RA and LA being used to derive the RLD signal which is being directed to channel 7 positive side and the onto the "patient".
Lead off detection is enabled on RA and LA electrodes with the comparators activated and the threshold set at 70%-30%. DC lead off is used with 24nA current sources.
CONFIG1 = 0b00000110
CONFIG2 = 0b00000010
CONFIG3 = 0b11001100
LOFF = 0b11101111
CH1SET = 0b10010001
CH2SET = 0b10010001
CH3SET = 0b10010001
CH4SET = 0b10010001
CH5SET = 0b10010001
CH6SET = 0b10010001
CH7SET = 0b10010110
CH8SET = 0b00000000
RLD_SENSP = 0b10000000
RLD_SENSN = 0b10000000
LOFF_SENSP = 0b10000000
LOFF_SENSN = 0b10000000
LOFF_FLIP = 0b00000000
LOFF_STATP = read only
LOFF_STATN = read only
GPIO = 0b00001111
PACE = 0b00000000
RESP = 0b00000000
CONFIG4 = 0b00000010
WCT1 = 0b00000000
WCT2 = 0b00000000
// Schematic:
The schematic does not include the Lead Off comparator circuit that is internal to the ADS1298, but it is active as seen in the register values above:
Thanks in advance for your help.
Br. Casper