Other Parts Discussed in Thread: TM4C1294NCPDT, ADS125H02, MSP-EXP432E401Y
Tool/software: Code Composer Studio
Dear Forum Team,
I am able to test the ADS125H02EVM using Delta-Sigma ADC Evaluation software and checked the read and write registers functionality. As a part of development activity, I have some query, mentioned below-
(1.) Can we use the onboard TM4C1294NCPDT controller for development purpose using Blackhawk USB100V2 JTAG with CCS.
(2.) Is TivaWare_C_Series-2.1.4.178 library directly can be used with ADS125H02 Example Code provided(SPI drivers).
(3.) Need to test PT100(3Wire type), can you suggest pin connections to J1 connector.
(4.) Some sample connection to test 0 to 10 volt Analog input.
(5.) what are the changes /configuration required to use RTD and Analog input together using ADS125H02EVM.
Best regards,
Anuj