Hi
I am currently using ADS7953 chip in data acquisition and we are lookin at ways for powerdown and powerup.As I looked at the Datasheet I found that there are two methods to do it
Method 1 involves just setting DI05 bit in mode control register and the Chip will be powered down at the 16th falling edge clk of the next data frame.
Method 2 involves controlling thru GPIO 3 pin reset .
Method 2 has a clear procedure for powering up on CS falling edge with DI05 0 in the mode control register and GPIO3 is set to high .
So what is the procedure to Powerup the chip when only using the DI05 bit set power down method
Thanks
Sundara Ramanan