Hi Team
I posted one question about gain error, offset error before as following link.
It's been locked so I open a new thread here.
Though Joseph told me gain error won't have big change according to the change of FSR,
The customer wants to know concretely how much it deviates from the standard when doing actual machine evaluation.
From the data sheet, it can be read that it has the following characteristic values when FSR: ± 2.048V and Ta = 25 ° C.
・ TYP: 0.01%, MAX: 0.15%
How about the gain error with following condition? Thanks.
【Condition】
・ Ambient temperature: 25 ℃
・ Power supply voltage: 5.25V
・ FSR: 6.144V
・ DR: 250SPS
・ Input mode: single-end