I am considering the use of the ADS131M08 for a thermocouple based temperature sensor. I have the data sheet for the part, but have a number of questions.
1. Section 8.3.5 of the data sheet indicates that the master clock should be synchronous with the SPI SLCK. Assuming we are using the onboard oscillator, how is this synchronization accomplished?
2. Can you recommend a 2.048 MHz crystal operating in the same temperature range as the ADS131M08?
3. The device requires both analog and digital power supplies. Is it possible to use one power supply for both?
4. Section 6.3 indicates that the digital supply can range from 2.7 to 3.6 V (3 V nominal). However, Section 8.1 implies that the digital supply should be either 1.8V or 3.3V. Which is right?