Would the TPL1401 be adequate for dynamically controlling the RDRV current mirror of the LMG3410 GaN FETs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, my colleague, AK will be able to provide a more complete answer, but I will give this a shot.
My understanding is that this must shunt current to GND. The TPL1401 is great for the ratiometric division of a value, but in this case, I do not think you will be able to control the slew rate. You should consider the TPL0501-100.
Thanks,
Paul
Paul_Frost said:My understanding is that this must shunt current to GND.
Yes. Per TPL1401 datasheet:
Features:
FB pin for precision current sink applications
Isn't that the whole point for using this over a DAC? Figure 6-34 in TPL1401 shows sinking a load current.
If I'm mistaken, could you run by AK a possible solution like Circuit D with DACx3401 as described in the app note.
Hi,
TPL1401 can sink current up to 10mA. Having said that, in this application, we need to really know the value of incoming current into the RDRV pin of LMG3410 which is missing in the datasheet. Also if the RDRV is sensitive to any parasitic capacitance or inductance we need to know that as well.
Also please keep in mind that we will have power on delays for TPL1401 to set the voltage. We need to assess these constraints before going ahead with TPL1401.
Regards,
AK