Other Parts Discussed in Thread: ADS8860, ADS8920B
Hi expert,
Customer want to use ADC in hydrogen commercial vehicle. Could you recommend a suit device for us? Here are the requirements:
Input Voltage: -5 V~+5 V
Channel: 1/2(1 is better)
Resolution: >14bit
Max input signal frequency: 20kHz
Output Interface: SPI
REF: 4.096V(Better for internal)
Operation Temperature: -40~125C
Supply voltage: 5V
I find ADS8681 is almost suit those requirements. But it has a 2nd order LPF inside, –3-dB cutoff frequency for the filter is typically 15 kHz. The max input signal frequency is 20kHz. Can we turn it off?
Best Regards
Songzhen Guo