Other Parts Discussed in Thread: ADS7128, BP-ADS7128
Hi ,
Does the TLA2528 is having the same protocol than ADS7128 as BP-ADS7128 is the proposed tool for TLA2528?
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi ,
Does the TLA2528 is having the same protocol than ADS7128 as BP-ADS7128 is the proposed tool for TLA2528?
Thanks
Hello,
Yes, these devices have similar protocols, and the TLA2528 can be used on the BP-ADS7128.
Note that the ADS7128 has more features than the TLA2528. If those extra features not available on the TLA2528 are called on, then the device can respond oddly. But the features they share use the same registers.
We suggest evaluating the ADS7128 that comes on board the EVM if interested in the TLA2528 due to the thermal pad on the devices (may be difficult to swap out). They will show same performance (aside from the extra features)
Regards
Cynthia