This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS1293: ECG data

Part Number: ADS1293

Hi Team,

We use four electrodes (RA, LL, LA, V) without RL to measure the ECG waveform.

ECG register setting as below.

Our application is continuous receive ECG waveform. The following ECG waveform is supplied by ECG simulator.

It has abnormal data causes the peak noise on ECG waveform after 5 to 30 minutes.

Could you provide some suggestions to us?


  • Hi William,

    Thank you for the post.

    I'll check with the team and get back to you. Thank you for your patience. 

    Thanks

    -TC

  • Hi William,

    Thanks for the post. 

    Is the abnormal data you show happen regularly after 5 to 30 minutes or happen once in 5 to 30 minutes? Can you check to see if it is possible to use a fixed test signal from the ECG simulator to see if this abnormal data occurs as well? 

    Thanks.

    -TC