Has put forward the question 20 days ago, did not find any valuable technical support. Once again, hope to meet with technology and gives directions:
When sampling a fixed level, such as 2.5 V when using the 2.5/5/10 SPS ADS1256 accurately measured voltage of 2.5 V, but use other faster SPS ADS1256 measured voltage on the low side too much (only about 2.03 V when the measured 100 SPS; Higher SPS, the measured voltage lower). All channel, single-ended and differential problem is same.
I used cycle read mode according to the manual , waiting the DRDY is low, a new channel switching, read the previous conversion value...
from The official website, and then goto support E2E, a series of operations to today, nearly 20 days, problem a bit didn't get the response, professional TI experts where to find? help me!!!