This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Replies: 1
Views: 75
Part Number: DAC11001A
Dear Technical Support Team,
I'd like to make a analog output system with DAC11001A and Opeamp.
①
Is it possible to output ±15V with DAC11001A?
EVM has OPA828 for VREFP and VREFN and user guide describes ±15V supply to VCC on board.
This VCC makes VREFP and VREFN with OPA828.
②
Could you suggest the companion Opeamp for output buffer of DAC?
I'd like to make a ±25V output with Opeamp from ±15V of DAC.
I'm considering the LTC6090 and OPA455 and OPA462 etc.
Best Reagards,
ttd
Hi,
DAC11001A can be used to generate a maximum of +/-15V with the following conditions
VCC = 18V, VSS = -18V , REFp = +15V & Refm = -15V.
We need to have a head room of 3V from VCC to Refp and VSS to Refm. Hope this is understood.
For buffering reference, I recommend OPA827. For outputs also OPA827 will be a good choice.
Regards,
AK