Hello Guys,
Good day.
Our customer is using the ADS131M08 with an Xmega processor which is using 8 bit SPI. He selected the proper mode.
After the reset procedure he send a null command, followed by a dummy crc and 8 channel read out.
The status FF2800 is returned. So that seems ok.
As he understand it, he first send a command which is 3 bytes. first the MSB, then LSB and then a padding byte with 0.
After that the dummy CRC which are just 3 zero bytes, and then 8 channels which are 24 bytes with 0 value.
he got this :
00FF2800
000005BC
0005FF00
0000054E
etc.
the first byte is because internal he use dword. The null command (in total 10x3=30 nul bytes) should give the status register content which is 0500h.
But he gets : 0005FF00. What is this FF. He is expecting to get 0500xx
Can he assume that all registers have the reset value after a reset procedure?
Thanks in advance!
Art