Hello,
i'm experiencing high noise when the adc is set for sample rates higher than 20 sps.
At 5,10 and 20 sps the conversion is very stable and reflect the datasheet.
The system is designed to measure a thermocouple or signal in mV like the fig. 88 of the datasheet.
In my design RI1 and RI2 are 1K, CI_cm1 and CI_cm2 are 4n7, CI_diff is 47n.
The conditions are the following:
SYS0: 0x40 (PGA=4)
MUX0: 0x01
VBIAS: 0x01
MUX1: 0x30
IDAC0: 0x00
IDAC1: 0xFF
some conversion values are presented in the following table (50 mV applied at differential
20 sps 40 sps 1000 sps
12490 12436 12534
12489 12480 12381
12490 12534 12446
12490 12496 12655
12490 12570 12340
12490 12497 12647
Suggestions for improvement?
Regards
Alessandro