Replies: 2
Views: 31
Part Number: ADC12QJ1600EVM
Hi Team,
I have bought the ADC12QJ1600EVM and want to use it with ZCU102. I have gone through the Datasheet and got confused which JESD Mode I need to select to use all the 4 channels at 1350MHz.
Please provide me the example design if any for the 2020.2 version of vivado.
Hi Krishna G,
Please use JMODE6 which has 6 SERDES lanes and at 1350Msps your line rate will be 11137.5Mbps and will using 64b/66b encoding scheme. Alternatively you can use JMODE0 which has 8 SERDES lanes and at 1350Msps your line rate will be 10800Mbps and will using 8b/10b encoding scheme
Please let me know if
Regards,
Neeraj
In reply to Neeraj Gill:
Neeraj Gill
Thanks for your guidance. I have given request for the core generation for Custom IP to TI with JMODE 6.