I am having an issue where the ADS1256 loses it's calibration values. I suspect that the part is being reset, but I am not seeing any glitches on the VDD, AVDD or Reset lines. The Avdd is powered by +5V with 1uF capacitor. The Dvdd is powered by +3.3V with 0.1uF capacitor. The Reset line is driven from a microcontroller I/O line at +3.3V. Is there a recommended schematic checklist for this part or any other causes for this part to reset? Should circuitry be added to enable SCLK only when chip select goes low in the unlikely case that SCLK could reset the ADS1256 while communicating with other IC's on the SPI bus?