Other Parts Discussed in Thread: TSW30H84EVM, DAC34H84, TRF3705
Hello!
I recognized a frequency depending phase shift between the two LO signals on the output of the two RF paths of the TSW30H84EVM (see figure).
I used a constant on the DAC34H84 output to see only the behavior of the two TRF3705. I have used equal length very short lines for two LO input and RF output connections to measure the phase difference. I have used my own splitter (not that one installed on the TSW30H84EVM). The dynamic range and every other parameter of the device is very excellent and meets my specifications.
For measuring my Doherty PA the best would be that the LO phase difference between the two channels is nearly zero! I will compensate this in my FPGA design but the phase difference is very large and also frequency depending. Is this a normal variance between two TRF3705 modulator implementations or is this coming from the output matching of the TSW30H84EVM?
Greetings!