This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC7512 problem

Other Parts Discussed in Thread: DAC7512, SN74AHC541

I have a board with a DAC7512 on it; VDD is 3.3 volts (measured 3.2). SYNC, SCL & DIN are driven by a SN74AHC541. The dac output is stuck at 2.4 volts. SYNC and DIN toggle between 3.2 volts and ground. SCL switches from 3.2 to 2.4 volts when SYNC switches to ground and toggles between 2.4 and ground while the DIN is being clocked in and rises to 3.2 volts when SYNC switches to 3.2 volts.
 
Does this set of symptoms indicate damage due to static discharge? Is this part particularly susceptible to ESD damage?
  • Hi Gary,

    You are working too late on a Saturday I think!  Can you provide a schematic and screen shots of your communication interface with the DAC7512?  Your problem description does not necessarily indicate ESD damage, you may just have a simple communication setup issue.  Let us know what controller you are working with as well (an MSP430, an FPGA, something else?).

  • Below are the schematic and a screenshot of the sync and clock signals at the
    dac inputs during an update. These signals at the input of the `541 switch
    between 3.2 volts and ground.  I found that there was some droop on VCC
    during dac updates and I added a 10 uF cap across VCC and ground at the dac
    chip. It appears that the dac is drawing a lot of current when sync is low
    and hence has been damaged (the output is stuck at 2.4 volts). I installed
    the chip a few days ago and was reasonably careful then and while testing
    the board but, however, not wearing a ground strap. The adc portion of the
    board works OK though I did have to add pull-ups on the inputs to the AND
    gate.

    The plan is to connect this board to an FPGA but for now for testing it is
    connected to an MSP430 with a 4 MHz clock. The dac update code is shown
    below. SYNC and SCL are initialized high.

    static void dacNext(int dacVal)
    {
    int din, k;
        din = dacVal;
        P1OUT &= ~SYNC;
        for (k = 0; k < 16; k++)
        {
            if (din & 0x8000)
                P1OUT |= DIN;
            else
                P1OUT &= ~DIN;
            P1OUT &= ~SCL;
            P1OUT |= SCL;
            din <<= 1;
        }
        P1OUT |= SYNC;
    }

    My apologies for the quality of the schematic image. I tried several times but could not improve it.

     

     

     

  • At the far right, it shows it goes up after the signal.  Can you scope the DAC7512 pins  4 5 and 6 individually?  The schematic shows pin 6 inverting, which it seems to, and the other 2 seem to be held high ( inverted output to low after the DAC7512 ).  This would make me suspect both the DAC7512 and sn74ahc541 as possible culprits of a solid output rather than pulsed.  Also if you can swap the connectors to Din, SCld Sync so that each has a turn on the 4 MHz clock to ensure the signal is getting out of the sn74ahc541.

    Hope this brightens your Sunday,

    Eric

  • Well it hasn't brightened my Sunday much but I appreciate you interest in my problem.

    In the screen shot, the top trace is the clock signal and was that on pin 5 of the dac. The sync trace was probed at connector JP2 but I have verified that the signal at pin 6 of the dac is identical. The signal at pin 4 of the dac (DIN) is also identical to that at JP2. The code updates DIN about 100 usec before the falling edge of the clock; I don't think that has any bearing on this problem.

  • Gary, sorry to hear that.

    The sn74ahc541 works at each side eliminating it as a suspect.  That leaves any solder issues before calling the DAC as a burned component.  I hate to admit how many times my solder work wasn't up to standard and caused an issue or one of my " new " breadboards being corroded causing lack of signal.  The only thing left to test before calling it toast is to make * edited  to correct * Din high, Sync tied to ground  and tie  clock to the input  frequency and see if you get anything.

    " Level triggered control input (active LOW). This is
    the frame sychronization signal for the input data.
    When SYNC goes LOW, it enables the input shift
    register and data is transferred in on the falling
    edges of the following clocks. The DAC is updated
    following the 16th clock cycle unless SYNC is taken
    HIGH before this edge, in which case the rising
    edge of SYNC acts as an interrupt and the write
    sequence is ignored by the DAC7512. "

    Tomorrow is another day and an opportunity to make things better,

    Eric

  • Hi Gary,

    Did you resolve the issue with your DAC7512 setup?