Hi,
We are using the ADS6422 12 bit ADC and are using the pin programming mode. What are the correct voltage levels for the multi-level programming pins CFG 1-4 and SEN?
The ADS642x datasheet from the T.I. website (June 2007) specifies VDD, 5/8 VDD, 3/8 VDD or GND.
Another post for the ADS644x states that the voltages should be VDD, 5/6, 3/6 and GND (and that the ADS642x datasheet still needs to be updated - which it does). The ADS644x datasheet has been revised with these values for the CFG pins but still specifies the VDD, 5/8, 3/8, GND for the SEN pin.
The ADS64XX EVM Users manual (SLAU196) schematic indicates settings of VDD, 2/3 VDD, 1/3 VDD or GND (implemented with three 1Kohm resistor divider and jumpers) for CFG pins and SEN pin.
Which are the correct values to use for the ADS6422?
Thanks,
Bert