Other Parts Discussed in Thread: DAC34SH84
Hi,
After receiving the Verilog code for TSW1400 + DAC34SH84 from Ebenezer a few weeks back, I first compiled the code as-is using Quartus 13.1, and loaded it onto the TSW1400 simply by loading the raw bit file (.rbf) through the GUI. That doesn't work, it loads the firmware but then states that no firmware was loaded. I did modify the DAC34SH84.ini file to point to the "tsw1400_top" file instead of the "DAC_SAMPLE_WISE", so the GUI loaded my compiled file automatically, but it still did not recognize is as proper firmware once loaded.
The compiled .rbf file is also significantly smaller than the ones that came with the HSDCPro GUI, about 2 MB compared to 5.8 MB for the other bit files. Should the project that I was sent compile into a usable firmware bit file, or is something else required? Thanks again,
Daaf