Hello,
I am working on a design involving the THS8135 to drive an analog VGA output signal from a BT.656 input (1x10 bit input). My application requires a negative sync on green. The datasheet describes that the component "provides additional dc bias on R, G, B, and Y channels to provide headroom for negative sync insertion". Do I need to provide a negative supply to Vref (or another pin) to have the analog output drive to -300 mV, or do I need an external DC bias circuit to adjust the voltage such that 0 V is -300 mV? If so, do you have an example design? I looked at the THS8135EVM schematic, but that board did not support a negative sync.
Thanks for your time.