I am using ADS7828E with Vdd at 3.3V as shown in the attached image. After some amount of successful run time, the ADC will inevitably fail and output a constant value - not the same output every time. When this happened originally, the Vdd pin dropped to 2.2V drawing 100mA. After lowering the resistor in series with the supply to 5 ohm and adding an additionally bypass cap, we thought the problem was solved. However, the unit still inevitably fails, but now the voltage drops to 2.8V still drawing over 100mA.
We are considering removing the 5 ohm resistor in series with the power supply, as well as changing the bypass cap at Vref to somewhere between 1uF and 10uF. I'm not convinced that either of those will solve the problem.
Are there any known scenarios that would cause this issue?