Hello,
As SDO output is 3V by default, I would like to add circuit protection in order to clamp the output to 1.8V to avoid damage in case of error programming.
The datahseet says " A low-capacitance protection diode may also be added with the anode connected to the SDO output and the cathode connected to the desired voltage supply to prevent an accidental pre-configured read command from causing damage"
Is also suitable for the chip to put a zener (with Vzener=1.8V) between SDO and ground?
Thank you so much
Best regards