Other Parts Discussed in Thread: ADS1263
Hi,
I'm currently designing a device using the ADS1263 and I have a few questions concerning the chop mode funcitonality and the data rate.
My settings are the following:
- Data rate: 400 sps
- Filter: sinc3
- Chop mode: ON
- Programmed delay: 0ms
I understand that the chop mode performs 2 acquisition to cancel the offset voltage but it is not mentioned how it works internally.
More importantly in the specification you can read "As a result of the delay required by the digital filter to settle after reversing the inputs, the chop-mode data rate is less than the nominal data rate, depending on the digital filter order and programmed settling delay.".
Also, I get that the chop mode multiplies by 2 the setting time of the filter as stated here "Chop mode: latency = 2 · td(STDR)"
Can you tell me more about it ? I don't understand how the digital filter order impacts the data rate. Will the ADC performs its acquisition at 400 sps or will the data rate change ?
Does the chop mode requires to wait the whole time for the filter setting ? (for information the setting time for sinc3 filter at 400sps is 8ms)
Thank you in advance.
Julien