Hello,
I recently purchased a DAC34SH84 EVM board and a FMC-DAC-Adapter to connect the EVM to a FMC connector on a Xilinx board. The problem is that the DAC34SH84 has a 180 pin HSMC connector, but the FMC-DAC-Adapter card has a 160 pin HSMC connector. The two do not mate. The description of the evaluation board on the website says " The FMC-DAC-ADAPTER board available from TI enables the connection of the DAC34SH84EVM to the FMC header on Xilinx based EVMs."
I have looked for an alternative TI FMC adaptor card but none are suitable. Is it possible to obtain such an adaptor card?
Thanks for your time,
Andy