Part Number: ADS8866
Hi, my customer use ADS8866, the schematic is as following.Now the data is read abnormal. Is there any problem? Is there have an code example?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi user4768533,
Looking at your schematic, you are using "4-Wire CS Mode Without a Busy Indicator" mode of operation as mentioned in the data-sheet. I think there are certain things that will need some working around -
ADS8866 MSP430 (existing) MSP430 (should be)
DIN UCA0SIMO UCA0STE -- because DIN is chip select for the ADC
CNV UCA0STE xxx -- This pin determines start of conversion; I recommend timer output.
DOUT UCA0SOMI UCA0SOMI -- This connection requires no change.
SCLK UCA0CLK UCA0SCLK -- This connection requires no change.
Please refer to the diagram below for a connection schematic.
You can refer to the "4-Wire CS Mode Without a Busy Indicator" mode of operation as mentioned in the data-sheet.