Part Number: ADS5482
Other Parts Discussed in Thread: THS4513
Hi,
I need to measure a single ended signal with an ADC (14 or 16 bits) at 100MSPS (ideally powered in 3.3V but not compulsory). My signal can vary between 0V and 10V and I need to measure low level (different to 0V) and high level.
At this speed, I find only ADC with differential inputs like ADS5482.
One solution seems to connect INM to VCM, and my signal to INP. For that, I must divide my signal and add an offset to be in the range VCM +/- xx V (0.75V for the ADS5482).
With this solution, the input signal seen by the ADC at his INP input will be an unbalanced signal (could be VCM - 0.75V for low level and VCM for high level).
What will be the behavior of the ADC with an unbalaced input?
Is there a better solution to measure such a signal (single ended with a measure of low and high level)?
Thanks
Matthieu Baque