Part Number: ADS1210
Hi,
My customer is using ADS1210.
He has a issue.
It is A/D covert value is shift at being high temperature.
The input differential voltage (AINP-AINN) is 0.193V.
In case of 25 degrees, convert value is "4B4477h".
In case of 45 degrees, convert value is "491B80h".
This is big deference.
At first, I want to confirm circuit.
Especially, it is the circuit of input part.
Customer uses BIAS pin.
Does this circuit have problem?
Best regards,
Shimizu