Part Number: ADS1115
Good day all,
Hobbyist here.
I am going to use the ADS1115 to measure batteries in series as per diagram below:
As you can see, there is a switch on the positive leading to VDD (so I can turn the ADS1115 on and off).
(assume each battery is 1.2V so it does not exceed 5V)
My question is regarding AIN0 - AIN3. As the positive of each cell will be attached to AIN0 to AIN3 respectively, and GND is connected to the neg of the battery, will there be any draw on the battery through AIN 0 - AIN 4 and GND plane when the switch between BATT1 and VDD is in an "off" position?
Basically, I am wondering if there is going to be a gradual continuous draw on the batteries while the switch is off.
Thanks!