Part Number: ADS1278
I am collecting data from the ADS1278 in fixed position TDM mode. My receiver is configured to latch data on the rising edge of SCLK as the ADC should be shifting on the falling edge. Running acquisitions at 144kHz I am always seeing the MSB of DOUT1 equal to one and the remaining DOUT1 bits at expected values. Data from the other 7 channels looks correct. I do have DVDD set to 2V and IOVDD at 3.3V.
After looking closer at the datasheet trying to debug this I am starting to doubt that you can actually get 8 channels at 144kHz in TDM mode. According to the frame-sync timing specification the min CLK period in high speed mode is 27ns. If you assume 50% duty cycle on the clock that gives you 13.5ns. However the allowed DOUT MSB propagation delay can be up to 21ns. Assuming 8 channels at 24 bits and a period = 2 * propagation delay, the best you can guarantee is ~93kHz.
Can anybody confirm my suspicions that this part is sample rate limited in TDM mode or am I seeing something else?