Part Number: ADS122C04
Hello All,
The Pin connection I did from below figure.
I'm using 10k resistor value as a pull-up and have a selected 100 kbps speed for I2C.
I'm trying to interface ADS122C04 24-bit ADC with MSP430FR2311
I have written following algorithm:
1. Send Reset Command (0x10)
2. Write Configuration Register
a. Register 0 (0x40) = 0x81;
b. Register 1 (0x44) = 0x00;
c. Register 2 (0x48) = 0x00;
d. Regoster 3 (0x4C) = 0x00;
//Here I'm using Single short conversation mode and Single channel Read Mode
3. Send Start Command (0x08);
4.loop
{
Wait for DRDY Pin to transition low;
send Read Command (0x10);
}
The DRDY pin goes low after sending the start command.
Once the DRDY pin goes low, again it unable to go in high state.
The Above algorithm I have a implemented and I'm unable to receive the data from ADC.
Please be needful.
Regards,
Kelvin