Other Parts Discussed in Thread: TVP5150, TVP5154
Hi All,
I would like to ask a question on BT.656 mode output for CCD/CMOS sensors.
For a BT.656 stream that is converted from a real PAL/NTSC signal, two fields are NOT taken at the same time. But nowadays many BT.656 stream actually comes from CCD/CMOS sensors and does their fields in the digital stream also captured at different times?
I figure that the internal mechanism of these CCD/CMOS sensors could be:
- Integrate (on the intensity of light components, for example, the Bayer pattern) the optical signal on the pixel sensor arrary every 1/30 second.
- 2. After the optical integration
1) sample and quantitize for lines 1, 3, 5 ... 2k-1, generating SAV and EAV bytes, and then output
2) sample and quantitize for lines 2, 4, 6 ... 2k, generating SAV and EAV bytes, and then output
If this is indeed the their actual mode of operation, then neighboring fields belonging to single frame are actually taken at the same time. Is that correct?
Another question is that in VPFE or DM64x chips, is there any way for the interrupt service routine triggered by VDINT0 or VDINT1 to know the the field ID (whether the interrupt is coming from the top or bottom field)?
Sincerely,
Zheng