This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADC16DX370: Device ADC16DX370REMT need US re-export licence required?

Part Number: ADC16DX370

Device ADC16DX370RMET need US re-export license required?

If the parameters shown below are met or exceeded for the part ADC16DX370RMET with US ECCN 3A001. a. 5. A

if US re-export license is required pls support written/email confirmation)

 

For ECCN3A001. a. 5. a

1) Pls get manufacturer/Supplier written / e-Mail confirmation on the part ADC16DX370RMET, if it is 

1) "designed or modified" for military use,

2) Hermetically sealed and

3) Rated for operation in the temperature range from below -54 Degree Celsius to above +125 Degree Celsius

 

Now customer will be tested in the chamber with target system for device environments test, the chamber temperature can be changed -40 to 85 (some case 100 degree) with humidity, but target is guarantee up to 85 degree operation