Part Number: ADS5404EVM
Other Parts Discussed in Thread: FMC-ADC-ADAPTER
Is the connector on the ADS5404EVM an FPC connector? Is it compatible with Xilinx development boards like the ZedBoard?
Thanks,
-Chris
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ADS5404EVM
Other Parts Discussed in Thread: FMC-ADC-ADAPTER
Is the connector on the ADS5404EVM an FPC connector? Is it compatible with Xilinx development boards like the ZedBoard?
Thanks,
-Chris
Chris,
The ADS5404EVM has a 2 bank HSMC connector. I am not sure what connector the Zedboard has. If it has a 2 bank HSMC connector, there is a good chance it will fit. If it has a 3 bank HSMC, TI makes a HSMC_ADC_Bridge board that would connect these two together. If the Zedboard has a FMC connector, TI has a FMC-ADC-Adapter that would connect these together.
Regards,
Jim
Thanks Jim!
For future users: the Zedboard has an FMC connector. The ADS5404EVM will NOT connect directly to the ZedBoard, the FMC-ADC-Adapter mentioned by Jim above will be required.
I ended up purchasing the AD9434-FMC-500EBZ development board from Analog Devices instead. It has an FMC connector and plugs directly into my ZedBoard without requiring an additional adapter card.