This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DAC60004: Change device from AD5024 to DAC60004

Part Number: DAC60004

Dear Technical Support Team,

I'd like to change device from AD5024 to DAC60004.

These are similar timing chart of SPI and command and electric characterization.

Is it easy to change?

If you have some advice , please let me know.

Best Regards,

ttd

  • Hi TTD,

    The DAC60004 and AD5024 have nearly identical register maps and timing. In fact, the TSSOP ,14-pin AD5064 variant of the family is pin for pin identical with the DACx0004 family and can be replace with no changes.

    The DACx0004 features an SDO pin that can handle readback commands, which is not featured on the AD5024. This will not effect the behavior of the system though, but can be added as feature if you want.

    Thanks,
    Paul