Part Number: DAC8771
Hi ,
Our customer has a question about DAC8771.
Does this device work properly under the following conditions?
Does this device work properly under the following conditions?
Iout & Vout shorted
Iout load resister opened
POC is set
Buck / Boost ON( full tracking mode)
The typical usage assumes a 500 ohm resistor.
However, end users may open the load.
So they did a test to open the load.
But this device broken...
I believe this device is not broken, as the load OPEN is usually a condition.
If POC clear (default), the device is not broken. The customer also said that the current value is correct.
In order to solve this problem, I will check the customer with the necessary information.
Can you give me some advice on what to check?
Can you give me some advice on what to check?
Best regards,
Hiroshi