Other Parts Discussed in Thread: DAC3484, , DAC3482, CDCE62005
I am experimenting with the DAC3482EVM w/ TSW1406 pattern generator. I am attempting to setup the WCDMA example outlined in the DAC348x EVM User's with limited success. I am running the both software programs with administrator permissions. I want to be clear that I follow the instructions in the User's manual quite literally and I do not alter any registers after loading the register file "DAC3484_FDAC_1228p8MHz_4xint_NCO_30MHz_QMCon.txt". I also load the WCDMA samples into HSPRO from the file "WCDMA_TM1_complexIF30MHz_Fdata307.2MHz_1000.tsw". After doing so, the spectrum of the signal that I observe is quite erradic, as if the samples are being garbled in the FIFO.
After observing this output spectrum behavior, I editted the registers through the GUI software to enable the FIFO alarms in the "advanced" tab. After clearing their status with the check box, the FIFO alarms remain set - e.g. FIFO collisions. I *think* toggling the "SIF SYNC" is supposed to reset the FIFO pointers but that does not resolve the FIFO alarms I observe. Based on the register loading from the file, I believe the input and output FIFO rates should be equal so I'm not sure why the collisions should be happening so frequently - if I am interpretting the alarm registers correctly. Maybe I am not properly resetting the FIFO pointers???
Any recommendations you can offer would be greatly appreciated.
-Chris