Part Number: ADC3244EVM
Other Parts Discussed in Thread: ADC3244
I'm using ADC3244 EVM, running it by default settings (two-wire mode). Given 60MHz CLKIN, I got 30MHz FCLK and 210MHz DCLK. The analog input channel is driven by constant voltage.
According to the datasheet, the ADC samples should be repeated(given constant input) every half cycle of FCLK, however, what I observe is the DA0 and DA1 are changing with a full cycle of FCLK. And my DAout keep changing between value 024a and 2ad4. It should be held stable.
Also another problem: my ADC3244EVM with Maximum supporting frequency as 125MHz, it seems it can not work in low CLKIN below 50MHz. When I apply CLKIN under 50MHz (like 30MHz), the FCLK and DCLK will get wrong.
Any idea why this happens? could it be a hardware problem, or am I missing something? Any prompts will be appreciated!
And when the CLKIN is above 50MHz, although DCLK and FCLK seem to work properly. The ADC3244EVM all Jumpers and registers configurations are set as default without changes. After I power on the EVM, I can see LED light-up indicate the 5V power supply, and I check the VADD and DADD, they are 1.8V as expected.
Best,
Yawen