Part Number: ADS1258
Hi,
We are using ADS1258 in our design. Able to write and read register ADS1258 registers (00h-09h).
ADC channels from AIN0 to AIN15 need to operated as single ended channels. We have configured the ADS1258 registers as below.
CONFIGO -0X3A.
CONFIG1 -0X83.
MUXSCH -0XFF.
Reference voltage applied is 5V.
Required hardware signals START and DRDY are taken care. After the above ADC register configuration, START signal (18 micro sec) is being applied from host and after 36 micro secs DRDY goes low, then Channel data read command 0x30 has sent to ADS1258 and received 4 bytes (including status byte) of data from ADC.
We are facing the below issues.
1. What ever the voltage applied at channel input (0v or 5v), Channel data is same and it is 0x7FFFFF.
2. How to know that, received to belongs to which channel?
Thanks,