Other Parts Discussed in Thread: LM27762, TPS727, TPS61099, ADS1261
Can you advise on the ideal power components for a 5v reference on the ADS1262 with a single 3.6v battery? Specifically for running a loadcell.
There are a ton of converters to boost the voltage, but in a previous thread it was suggested to boost the voltage to 5.3 and then drop it back down to 5 with a LDO. I'm assuming this is to smooth over the voltage and provide a nice clean reference. Are there any single chip components? if not, what would be the ideal components for such a setup.
I am running everything else at 3.3v. The only 5v usage would be for the reference on the ADS1262/Loadcell. Accuracy of the loadcell reading is more important than efficiency (it is a battery application, so efficiency within reason)